SLUUAV7C December 2013 – November 2022 BQ40Z50 , BQ40Z50-R2
The Board Offset calibration option is not offered in Battery Management Studio, because it is not required when using the bq40z50EVM. The Board Offset calibration option is available in bqProduction.
Current can also be calibrated using the FETs. Measure the current in the discharge path and enter this value in the Applied Current field.