SLUUB41A May 2014 – October 2021 BQ76920 , BQ76930 , BQ76940
The data sheet states that adjacent cells should not be balanced simultaneously. The part does not restrict selection of adjacent cells.
Whether it is safe depends on which cells are balancing and the cell voltages. If 2 adjacent cells are balanced, the VCx pin between the cells does not change significantly in voltage. The differential input voltage of the next cell effectively doubles. If voltages impressed on the device are within the absolute maximum limits (both single-ended and differential), this is okay.
As an example, assume all cells are at 4 V. If cells 4 and 5 are balanced, the VC3 input pulls to VC4, which is approximately the cell 4 voltage or 16 V. This is within the single-ended absolute maximum voltage of 3 × 7.2 = 21.6 V. VC3-VC2 voltage doubles, or is 8 V; this is within the 9-V absolute maximum differential voltage for this input pair. So this balance combination should be okay. However, if cell 1 and cell 2 are balanced, VC0 pulls to the cell 1 value of 4 V. Because this is above the absolute maximum of 3.6 V, this combination of balancing could damage the device and should not be selected.
As another example, if the cell voltages are 3.6 V, the absolute maximum on VC0 from the above example would not be violated, and cells 1 and 2 could be balanced at the same time. However, if cells 4 and 5 were also simultaneously selected for balancing, VC2 would be approximately the cell 1 voltage of 3.6 V and VC3 would be approximately the cell 4 voltage of 14.4 V. VC3-VC2 would be 10.8 V and would exceed the absolute maximum of 9 V.
When external balancing is used, the control voltage for the external FETs is developed across the input resistor. With adjacent cells selected for balancing, one of the FETs may not receive an adequate control voltage and its balancing will be ineffective.
Adjacent cells in adjacent groups may be balanced simultaneously, for example cells 5 and 6 with a BQ76930. Because the cells are in different groups, they have separate input resistors for each group and the balancing can operate independently, even with external balancing. Be cautious of common path resistances between groups. See Section 4 of the BQ769x0 Family Top 10 Design Considerations document for more information.
Because of the complexity of determining when adjacent cell balancing may be safe, the user should follow the data sheet recommendation.