This user's guide provides detailed testing instructions for the PWR664 evaluation modules (EVM) using the bq25890, bq25892, bq25895, bq25896 or bq25895M (bq2589x) devices. Also included are descriptions of the necessary equipment, equipment setup, and procedures. The reference documentation contains the printed-circuit board layouts, schematics, and the bill of materials (BOM).
Microsoft, Windows are registered trademarks of Microsoft Corporation.
For detailed features and operation, refer to Table 1 for a list of devices and their data sheets.
Device | Document |
---|---|
bq25890, bq25892 | SLUSC86 |
bq25895 | SLUSC88 |
bq25895M | SLUSCC8 |
bq25896 | SLUSC76 |
The bq2589x evaluation module (EVM) is a complete charger modules for evaluating an I2C-controlled single NVDC-1 charge using the bq2589x device.
This EVM doesn’t include the USB-to-GPIO interface board. To evaluate the EVM, a USB-to-GPIO interface board must be ordered separately.