SLUUBD4A April 2016 – November 2022 BQ27220
If the [OTD] condition exists for a time period that exceeds the OT Dsg Time, the BQ27220 device goes into an overtemperature discharge condition. This function is disabled if OT Dsg Time is set to 0.
In an overtemperature discharge condition the ChargingCurrent() is set to 0 and the [OTD] bit is set in the BatteryStatus() register.