SLUUBD4A April 2016 – November 2022 BQ27220
To use ot.fs files to configure the BQ27220 device on power up, do the following:
Step 1: Use the GPCCEDV tool (on ti.com) to generate the 7-point CEDV parameter and the 11-point loaded voltage points. Refer to the BQ27220EVM-744 User's Guide (SLUUBF5).
Step 2: Use the Battery Management Studio (BQStudio) software to finalize all the values for Calibration/Configuration/Gas Gauging in RAM based on the application.
Step 3:
Programming the OTP Profile 1:
Programming the OTP Profile 2:
Programming the OTP Profile 3:
Step 4: Use BQStudio to generate the ot.fs file, which contains I2C instructions (with data) on how to program the OTP with the values that were just setup in RAM.
Step 5: Use the ot.fs file with the SmartFlash programming tool; the OTP on the BQ27220 device can be programmed.