SLUUBG3B July 2016 – August 2021 TPS548D21
Voltage Source: The input voltage source VIN must be a 0-V to 18-V variable DC source capable of supplying at least 12 ADC. The external voltage source on the REFIN_TRK pin must be between 0.5 V and 1.25 V. Also, the output impedance of the external voltage source must be much less than 100 kΩ.
Multimeters: It is recommended to use two separate multimeters Figure 6-1. One meter is used to measure VIN and one to measure VOUT.
Output Load: A variable electronic load is recommended for testing Figure 6-1. It must be capable of 40 A at voltages as low as 0.6 V.
Oscilloscope: An oscilloscope is recommended for measuring output noise and ripple. Output ripple must be measured using a tip-and-barrel method or better as shown in Figure 6-2.The scope must be adjusted to 20-MHz bandwidth, AC coupling at 50 mV/division, and must be set to 1-µs/division.
Fan: During prolonged operation at high loads, it may be necessary to provide forced air cooling with a small fan aimed at the EVM. Temperature of the devices on the EVM must be maintained below 105°C.
Recommended Wire Gauge: The voltage drop in the load wires must be kept as low as possible in order to keep the working voltage at the load within its operating range. Use the AWG 14 wire (2 wires parallel for VOUT positive and 2 wires parallel for the VOUT negative) of no more than 1.98 feet between the EVM and the load. This recommended wire gauge and length should achieve a voltage drop of no more than 0.2 V at the maximum 40-A load.