Make sure that Section 5.3.6 is implemented for setting up all the equipment before starting the power-up
sequence. Figure 6-1
can be used as a reference.
Enable supply #1;
Enable supply #2 and #3, the quiescent current on DMM1 and DMM2 ranges from 1 mA to approximately 3 mA if everything is set correctly;
Enable the function generator, two-channel outputs: channel-A and channel-B;
There will be:
Stable pulse output on the channel-A and channel-B
in the oscilloscope (refer to Figure 6-1);
Scope frequency measurement is the same with function generator output;
DMM #1 and #2 read measurement results should be around 10 mA, ±2 mA under no load conditions. For more information about operating current, refer to the UCC21520 data sheet.
Figure 6-1 Example Input and Output Waveforms (Channels 3 and 4 are PWM Inputs, Channels 1 and 2 are Outputs)