SLUUBL7A February 2017 – February 2022 TPS543C20
To measure the efficiency of the power train on the EVM, it is important to measure the voltages at the correct location. This is necessary; otherwise, the measurements will include losses in efficiency that are not related to the power train itself. Losses incurred by the voltage drop in the copper traces and in the input and output connectors are not related to the efficiency of the power train, and they must not be included in efficiency measurements.
Test Point | Node Name | Description |
---|---|---|
TP14 | VOUT | Sense VOUT+ locally across C9. Use for efficiency and ripple measurements. |
TP3 | GND | Sense VOUT– locally across C9. Use for efficiency and ripple measurements. |
TP16 or TP18 | VIN | Sense VIN + across C14 or C26 |
TP35 or TP33 | GND | Sense VIN– across C14 or C26 |
Input current can be measured at any point in the input wires, and output current can be measured anywhere in the output wires of the output being measured. Using these measurement points result in efficiency measurements that do not include losses due to the connectors and PCB traces.