SLUUBT5C November 2018 – June 2021 BQ40Z80
This command sets the minimal voltage at the system power converter input at which the system will still operate. This command writes to the data flash value Min System Voltage. Write it once on the first use to adjust for possible changes in the system design from the time the battery pack was designed.
SBS Cmd | Name | Access | Protocol | Type | Min | Max | Default | Unit | ||
---|---|---|---|---|---|---|---|---|---|---|
SE | US | FA | ||||||||
0x5D | TurboEdv() | R/W | R/W | R/W | Word | mV |