SLUUBY1B December 2020 – April 2022 BQ76942
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Power | Shutdown | Shutdown Cell Voltage | I2 | 0 | 32767 | 0 | mV |
Description: Configures the cell voltage threshold at which the device will enter SHUTDOWN mode. This threshold does not apply to VC pins configured as interconnects.
Note: Consider setting this parameter to zero if the cell open wire feature is enabled, since an open wire will result in a low voltage on the disconnected cell, and the device may shut down before the open wire event is recorded.
0 = Cell-Voltage-based shutdown disabled
All other values = Cell voltage shutdown threshold