SLUUBZ9 May 2020 TPS92200
Figure 6 shows the output current ratio to the full-scale output current versus VDIM voltage level in analog dimming mode. VIN = 12 V, 1 White LED is used as load. The LED current is set at 1.0 A with VDIM=1.2V.
Figure 7 shows the output current ratio to the full-scale output current versus PWM duty cycle in analog dimming mode. VIN = 12 V, 2 White LEDs in series used as load. The LED current is set at 1.0 A with 100% PWM duty. PWM frequency is 50 kHz.