Some of the tasks the user can perform with the
GUI include:
- Turn on or off the power supply output, either through the hardware control line or the PMBus operation command.
- Monitor real-time data that is continuously monitored and displayed by the GUI:
- Input voltage
- Output voltage
- Output current
- Die temperature
- Warnings and faults
- Configure common operating characteristics such as the following:
- VOUT trim and margin
- UVLO
- Soft-start time
- Warning and fault thresholds
- Fault response
- On/off modes