SLUUC48A February 2020 – February 2022 TPS546B24A
The default configuration of the EVM is for 2-phase operation. For a single-phase operation, modify the EVM as follows:
This will leave the AVIN (pin 26) of U1_P2 powered. If no-load leakage current or light-light efficiency measurement is important, the U1_P2 AVIN pin should also be disconnected from the input supply. Disconnect the loop follower U1_P2 AVIN from VIN by removing the jumper from JP7_P2.