SLUUC57B october 2019 – august 2023 BQ79600-Q1
The physical setup for the GUI is the same as for the microcontroller, but instead uses an USB2ANY interface and 10-pin cable for the UART/SPI connections on J4. The USB2ANY has a USB Mini-B connector on the right side. Plug the provided USB cable (or any USB cable with a Mini-B connector) into the USB2ANY. Plug the other end of the cable (USB ‘A’) into the computer. Then connect the 10-pin connector cable to J4 of the USB2ANY (middle most connector) and the key side must be facing upwards when connecting to the EVM header J4. Refer to the figure below and this is explained in more detail in the USB2ANY user guide and the BQAutoEval GUI user guide.