SLUUC57B october 2019 – august 2023 BQ79600-Q1
The EVMs are connected using the female connectors J7 and J9 on the bottom side of the BQ79600EVM and the male connectors J2, J3, J4, and J5 on the top side of the LAUNCHXL2-TMS57012 LaunchPad™. Connect the J7 20-pin female connector on the bottom side of the BQ79600EVM to the J2 and J3 10-pin male connectors on top side of the LAUNCHXL2-TMS57012 LaunchPad™, and J9 20-pin female connector on the bottom side of the BQ79600EVM to the J4 and J5 10-pin male connectors on the top side of the LAUNCHXL2-TMS57012 LaunchPad™, as shown in the following figure. By default, the TMS570 LaunchPad is powered by the USB port on the host computer. Remove JP1 from the LaunchPad for correct operation.
The microcontroller is used to supply VIO voltage to the device. The user can select either the 3.3-V or 5-V option. To use 3.3 V, make sure that JP2 on the microcontroller LaunchPad is connected and set jumper J6 in the 1-2 position (this is the default configuration on the EVM). To use 5 V, verify that JP3 on the microcontroller LaunchPad is connected and set jumper J6 in the 2-3 position.