All trademarks are the property of their respective owners.
The TPS546B24AEVM-1PH evaluation module uses the TPS546B24A device in a buck design. It designed for a nominal 12-V bus and to produce a regulated 1.2-V output at up to 20 A of load current. The TPS546B24AEVM-1PH provides a number of test points to evaluate the performance of the device.
The following warnings and cautions are noted for the safety of anyone using or working close to the TPS546B24AEVM-1PH. Observe all safety precautions.
![]() | Warning | The TPS546B24AEVM-1PH circuit module may become hot during operation due to dissipation of heat. Avoid contact with the board. Follow all applicable safety procedures applicable to your laboratory. |
![]() | Caution | Do not leave the EVM powered when unattended. |
The circuit module has signal traces, components, and component leads on the bottom of the board. This may result in exposed voltages, hot surfaces, or sharp edges. Do not reach under the board during operation.
The circuit module may be damaged by over temperature. To avoid damage, monitor the temperature during evaluation and provide cooling, as needed, for your system environment.
Some power supplies can be damaged by application of external voltages. If using more than 1 power supply, check your equipment requirements and use blocking diodes or other isolation techniques, as needed, to prevent damage to your equipment.
The communication interface is not isolated on the EVM. Be sure no ground potential exists between the computer and the EVM. Also be aware that the computer is referenced to the battery- potential of the EVM.