SLUUCA9A September 2020 – April 2021 TPS546B24A
When the Monitor screen (Figure 10-10) is selected, the screen changes to display real-time data of the parameters that are measured by the device. This screen provides access to:
With two devices stacked together, the Iout reading is the total load supported by both devices. There is also an Iout which shows the current in each phase.