The default configuration of the EVM is for single
rail input. Split rail input enables operation with 3.3V PVIN. For split rail
operation, configure the jumpers on the EVM as follows:
- Move the jumper JP3 to position 1-2 to disconnect the AVIN pin
from the PVIN pin.
- Apply the AVIN input to T1. 4-V or greater AVIN is required to
bring the VDD5 voltage high enough to enable conversion.
- If operation with 3.3-V PVIN is needed and the EN Select jumper (JP4) is in
position 3-4, the resistor divider at the EN/UVLO will need to be changed.
Alternately move the EN Select jumper to position 1-2 and use the control signal
to enable conversion or use the On/Off Config and OPERATION
commands to enable conversion.