SLUUCD4 April 2021 TPS92682-Q1
Click Next > to install.
Click Next > to accept the License Agreement.
Select Full Install and click Next > to install the evaluation software, the UniFlash, and the required XDS drivers. Full installation for both Windows 10 and 7 are provided.
If .NET Framework 4.5 or higher does not exist on the computer, the .NET Framework installation begins. Installation of .NET Framework will take several minutes. If .NET Framework 4.5 or higher exists on the computer, the installation jumps to the XDS driver installation.
A window appears indicating the completion of the .NET Framework installation.
Click Next > to continue the installation.
Click Next > to install the XDS driver.
The completion of the XDS driver installation is shown in Figure 6-8.
The TI-Emulators installation starts at this point. This will install the necessary drivers for running the application. In the next few steps as shown in Figure 6-9, Figure 6-10 and Figure 6-11 click Next > to perform the installation.
Accept the license agreement in Figure 6-10.
In the next few windows click Next >, and if prompted by Windows Security about software installation as shown in Figure 6-12, select Install.
The screen showing the completion of the TI Emulators installation is shown in Figure 6-13. Click Finish to move to the next step.
The UniFlash installation starts at this point. UniFlash is required to program the LaunchPad. In the next few steps as shown in Figure 6-14, Figure 6-15 and Figure 6-16 click Next > to start the installation.
When UniFlash installation completes, click Finish to launch the UniFlash and program the LaunchPad.
Figure 6-18 shows the completion notification of the TPS92682-Q1 Evaluation Software. Deselect the Launch Application and click Finish.