SLUUCH0 April   2022 LMR51430

 

  1.   Trademarks
  2. 1Introduction
    1. 1.1 Description
    2. 1.2 Features
  3. 2EVM Setup
    1. 2.1 Adjusting the Output Voltage
  4. 3PCB Layouts
  5. 4Schematic
  6. 5LMR51430EVM Bill of Materials

EVM Setup

This section describes the jumpers and connectors on the EVM and how to properly connect, set up, and use the LMR51430EVM.

    VIN – Terminal TP1 Power input terminal for the converter. Adjacent to it is the GND reference ground. Use this terminal to attach the EVM to a cable harness.
    EMI IN+ – Terminal TP13 Input terminal for input filter of the converter. If an input filter is desired between the supply voltage and the LMR38020, connect the supply voltage between EMI IN+ and EMI GND (Terminal TP14) on the bottom layer.
    VOUT – Terminal TP6Regulated output voltage for the converter. Adjacent to it is the GND reference ground.
    GND – Terminal TP2, TP5, TP7, TP14Ground reference for the converter. Use these terminals to attach the EVM to a cable harness.
    ENABLE SETTING – Jumper J1Used to enable the switch-mode converter. The device will be enabled when the EN pin is high, and disabled when low.
Figure 2-1 Enable Jumper Setting
    Jumper J4Replacing J4 with a wire can use current scope to test the inductor current.