SLUUCH4A October 2021 – October 2023 BQ27Z746
Standard commands are common commands from the Smart Battery Specification (SBS) industry-standard which defines smart battery interfacing. Standard commands use a command code pair to associate the registers associated with each command. Read and write commands should be addressed to the LSB of the command code.
Example: Read the RelativeStateOfCharge.
Figure 9-1 shows 0x2E 00 in the Data column of the Transaction Log sub-window. This value is 46 in decimal, corresponding to the SOC% shown in the DashBoard window to the right.