SLUUCH6B september 2022 – september 2023 TPS543B22
The TPS543B22EVM is provided with input connectors, output connectors, and test points as shown in Table 3-1 and Table 3-2.
To support the minimum input voltage with the full rated load on both outputs with the default EVM, a power supply capable of supplying greater than 20 A must be connected to J1 through a pair of 18-AWG wires or better.
For U2, the load must be connected to J2 and for U1, the load must be connected to J14. Two pair of 18-AWG wires or better must be used for each connection. With the maximum current limit setting, the maximum load current capability is near 20 A before the TPS543B22 goes into current limit. Wire lengths must be minimized to reduce losses in the wires.
Test point TP30 provides a place to monitor the VIN input voltage with TP33 providing a convenient ground reference for U1. Test point TP2 provides a place to monitor the VIN input voltage with TP9 providing a convenient ground reference for U2. TP31 is used to monitor the output voltage of U1 with TP36 as the ground reference. TP1 is used to monitor the output voltage of U2 with TP16 as the ground reference.
If modifications are made to the TPS543B22EVM, then the input current can change. The input power supply and wires connecting the EVM to the power supply must be rated for the input current.
REFERENCE DESIGNATOR | NAME | RELATED IC | FUNCTION |
---|---|---|---|
J1 | VIN | Both | VIN screw terminal to connect input voltage (see Table 1-1 for VIN range). |
J2 | VOUT_P2 | U2 | VOUT screw terminal to connect load to output. |
J3 | VOUT Select | U2 | VOUT selection header. Use shunt to set output voltage. See Table 2-1. |
J4 | ENSYNC_P2 | U2 | 2-pin header to connect U2 buffer output enable to ground. Populate shunt to enable output of buffer. Remove shunt to make buffer output high impedance. |
J6 | VO_2NDSTG | U2 | Output Second Filter. |
J7 | FSEL Select | U2 | FSEL selection header. Use shunt to select FSEL resistor. See Table 2-2. |
J8 | FSEL Test | U2 | Test mode 1-2 use pin strap resistors. 2-3 I2C test mode. |
J9 | MODE Select | U2 | MODE selection header. Use shunt to select MODE resistor. See Table 2-3. |
J10 | MODE Test | U2 | Test mode 1-2 use pin strap resistors. 2-3 I2C test mode. |
J14 | VOUT_P1 | U1 | VOUT screw terminal to connect load to output. |
J15 | EN_OFF_P1 | U1 | 2-pin header for enable. Add shunt to connect EN to ground and disable device. |
J16 | ENSYNC_P1 | U1 | 2-pin header to connect U4 buffer output enable to ground. Populate shunt to enable output of buffer. Remove shunt to make buffer output high impedance. |
REFERENCE DESIGNATOR | NAME | RELATED IC | FUNCTION |
---|---|---|---|
TP1 | VOUT_P2 | U2 | VOUT test point. Use this for efficiency, output regulation, and bode plot measurements. |
TP2 | VIN_P2 | U2 | VIN test point. Use this for efficiency measurements. |
TP3 | SW_P2 | U2 | SW node solder mask opening. |
TP4 | VDRV_P2 | U2 | VDRV node test point. |
TP5 | SW_P2 | U2 | SW node test point. |
TP6 | PGOOD_P2 | U2 | PGOOD test point. |
TP7 | MSEL_P2 | U2 | MODE test point. |
TP8 | AGND_P2 | U2 | AGND test point. |
TP9 | PGND_P2 | U2 | PGND test point. |
TP10 | VCC_BUF_P2 | U2 | VDRV Voltage Supply to Buffer. |
TP11 | GOSNS | U2 | Remote Sense for U2. |
TP12 | FSEL_P2 | U2 | FSEL test point. |
TP13 | PGND | U2 | Ground near P2 SYNC input. |
TP14 | BODE-_P2 | U2 | Test point between voltage divider network and output voltage. Used for Bode plot measurements. |
TP15 | BODE+__P2 | U2 | Used for Bode plot measurements. |
TP16 | PGND_VO2_P2 | U2 | PGND test point. Use this for efficiency measurements. |
TP17 | EN__P2 | U2 | EN test point. If user is applying an external voltage, then the external voltage must be kept below the absolute maximum voltage of the EN pin of 6 V. |
TP18 | SYNC_P2 | U2 | SYNC test point. Supply an external clock to this test point to synchronize U1 regulators. |
TP19 | VO_2NDSTG | U2 | SMB connector to measure output voltage after second stage filter if added to EVM. When using this test point, the scope must be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP20 | VO2_PGND | U2 | Ground for second stage filter output. |
TP21 | ISNS | Both | Test point to measure current in load transient circuit. Gain is 20 A/V. |
TP22 | FGEN | Both | Test point to connect function generator to load transient circuit. Slowly increase amplitude and vary slew rate of function generator for desired load step. |
TP23 | ISNS | Both | Test point to measure current in load transient circuit. Gain is 20 A/V. |
TP24 | SW_P2 | U2 | SMB connector to measure SW node. When using this test point, the scope must be set for 50-Ω termination. The combination of 50-Ω termination and 450-Ω series resistance creates a 10:1 attenuation. |
TP25 | VOUT_P2 | U2 | SMB connector to measure output voltage. When using this test point, the scope must be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP26 | VO_2NDSTG | U2 | Test point to measure output voltage after second stage filter if added to EVM. |
TP27 | PGND | Both | PGND test point for load transient circuit. |
TP29 | VOUT_P1 | U1 | SMB connector to measure output voltage. When using this test point, the scope must be set for 1-MΩ termination. When using 50-Ω termination, a 2:1 divider is created. |
TP30 | VIN_P1 | U1 | VIN test point. Use this for efficiency measurements. |
TP31 | VOUT_P1 | U1 | VOUT test point. Use this for efficiency, output regulation, and bode plot measurements. |
TP32 | EN_P1 | U1 | EN test point. If applying an external voltage, then the external voltage must be kept below the absolute maximum voltage of the EN pin of 6 V. |
TP33 | PGND_P1 | U1 | PGND test point. |
TP34 | PGOOD_P1 | U1 | PGOOD test point. |
TP35 | AGND_P1 | U1 | AGND test point. |
TP36 | PGND_P1 | U1 | PGND test point. Use this for efficiency measurements. |
TP37 | VO_SNS | U1 | Used for Bode plot measurements. |
TP38 | BODE-_P1 | U1 | Test point between voltage divider network and output voltage. Used for Bode plot measurements. |
TP39 | VCC_BUF_P1 | U1 | VDRV Voltage Supply to Buffer. |
TP40 | PGND_P1 | U1 | PGND test point. |
TP41 | SYNC_P1 | U1 | SYNC test point. Supply an external clock to this test point to synchronize U4 regulators. |