SLUUCI9A January 2022 – December 2022 UCC28781
Safety: This evaluation module is not encapsulated and there are accessible voltages that are greater than 50 VDC.
Voltage Source: Line-Isolated DC source capable of handling 100-W power level. Set output current limit to 1 A.
Input Isolation Transformer: If the DC source has no internal safety isolation from the AC line, a suitably-rated 1:1 isolation transformer shall be used on the input to the DC source and be constructed in a manner in which the primary windings are separated from the secondary windings by reinforced insulation, double insulation, or a screen connected to the protective conductor terminal.
Output Meters: Digital voltage meter, digital current meter
Input Meters: Digital voltage meter, digital current meter
Oscilloscope:
Output Load: Resistive or electronic load capable of handling 100 W at 15 V.
Recommended Wire Gauge: Insulated 18AWG.
Set up the test configuration for DC input as shown in Figure 7-1.
Caution: Do not leave EVM powered when unattended.
!! Do not apply an AC voltage source to the DC input of this board. This will damage the EVM! (See above set-up of Voltage Source)