SLUUCJ6 November 2023
Most of the configuration of the BQ76907 is accomplished through setting values in the data memory. The data memory locations are accessed using the buttons in the Data Memory view. The Parameter View selection at the top of the panel allows the choice of basic parameters which shows commonly used parameters, or all parameters which shows more configuration parameters. Data values may be changed by selecting and entering a value. Parameter registers, which are bit fields, may be changed by selecting the bit in the pop up when the register or its value is selected. Data Memory must be written after bit changes, a button is provided under the bit field to write to Data Memory. Figure 3-6 shows the bit field for the Enabled Protections A which is one of the most basic settings that must typically be changed with the EVM.
Changes to configuration by memory changes take place immediately, however the FETs are enabled using the FET_ENABLE command. Enabling a protection and enabling the protection action on a FET are not sufficient, the FETs must be enabled with the command.
The Export tool in the Data Memory view can be used to save the configuration data to a comma-separated-value file format which can be accessed by a spreadsheet program. Reading data before exporting with the Read All button loads the data from the part rather than values which may be only in the view. The Import tool allows loading a saved file into the view so that it can be written to the device. The Write All tool writes all values in the view, into registers in the device.