SLUUCJ6 November 2023
The Commands tab is displayed on the right side of the BQStudio window. Buttons in this panel allow the use of commands that can be used for reading various information about the device and for certain operations. Commands and returned data are shown in the Log Panel of the tab. The seal function is unusual in general evaluation and is not recommended during initial evaluation.
Sealing the device without remembering the key reduces the function of the EVM.