Use the following instructions to perform the
overcurrent test on the TPS48111Q1EVM:
- Pre-charge theoutput voltage by following the steps in Pre-charging Functional
Test.
- Now, enable the control input INP (TP6) of the main MOSFETS.
- Disable the pre-charge FET by connecting INP_G
(TP24) to ground.
- By default, the EVM is configured for 5-A
overcurrent protection.
- Now, load the output with rheostat or electronic
load and gradually increase the load current to observe the overload behavior of
TPS48111-Q1.
- Place jumper J3 at other settings to test at
various overcurrent limits.
Figure 5-7 and Figure 5-8 show test
waveforms for an overcurrent fault.
Figure 5-7 Overcurrent Response of
TPS48111-Q1 for a Load Step from 2 A to 8 A With 5-A Overcurrent Protection
Setting
Figure 5-8 Auto-Retry Response of
TPS48111-Q1 for an Overcurrent Fault