Some of the tasks the user can perform with the
GUI include:
- Turn on or off the power supply output, either through the hardware control line or the PMBus operation command.
- Monitor real-time data. Items such as input voltage, output voltage, output current, die temperature, and warnings and faults that are continuously monitored and displayed by the GUI.
- Configure common operating characteristics such as the following:
- VOUT trim and margin
- UVLO
- Soft-start time
- Warning and fault thresholds
- Fault response
- On/Off modes
This software is available for download at http://www.ti.com/tool/fusion_digital_power_designer.