This manual discusses the BQ40Z50-R5 device's modules and peripherals, and how each is used to build a complete battery pack gas gauge and protection solution. See the BQ40Z50-R2 1-Series to 4-Series Li-Ion Battery Pack Manager data sheet (SLUSCS4) for BQ40Z50-R5 electrical specifications, and the BQ40Z50-R4 to BQ40Z50-R5 Change List to see the new BQ40Z50-R5 features and performance improvements.
The following notation is used if SBS commands and data flash values are mentioned within a text block:
The reference format for SBS commands is: SBS:Command Name(Command No.): Manufacturer Access(MA No.)[Flag]; for example:
SBS:Voltage(0x09) or SBS:ManufacturerAccess(0x00): Seal Device(0x0020)
Impedance Track™ is a trademark of Texas Instruments.
Impedance Track® is a registered trademark of Texas Instruments.
All trademarks are the property of their respective owners.
The BQ40Z50-R5 device provides a feature-rich battery management solution for 1-series cell to 4-series cell battery-pack applications. The BQ40Z50-R5 device has extended capabilities, including: