SLUUCN4A January 2023 – February 2024
The BQ40Z50-R5 device can be configured to shut down when the RSOC is less than the RSOC threshold specified in Low RSOC SD Threshold for more than the time interval specified in Low RSOC SD Time. Setting PowerConfig[RSOC_SD] = 1 enables this feature. Once the timer start, only a charge current detection event will restart the timer. When the timer reaches Low RSOC SD Time, the time-based shutdown effectively triggers the MAC shutdown command to start the shutdown sequence. The BQ40Z50-R5 device returns to NORMAL mode when voltage at PACK pin > VSTARTUP.