SLUUCN4A January 2023 – February 2024
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Calibration | Interconnect Resistance | Cell 1 | I2 | 0 | 1000 | 0 | mΩ |
Description: This is the interconnect resistance value entered by the user that represents the interconnect resistance between the negative rail and the bottom of Cell 1, plus the interconnect resistance of the connection from the bottom of the first cell to the gauge. The measured CellVoltage1() is compensated for the voltage drop introduced by this resistance.