SLUUCN4A January 2023 – February 2024
This command enables ManufacturerInfoC read/write on ManufacturerBlockAccess() and ManufacturerData() in SEALED, UNSEALED, and FULL ACCESS modes.
Status | Condition | Action |
---|---|---|
Activate | 0x007B to ManufacturerAccess() | Output 32 bytes of ManufacturerInfoC on
ManufacturerBlockAccess() or ManufacturerData() in
the following format:
AABBCCDDEEFFGGHHIIJJKKLLMMNNOOPPQQRRSSTTUUVVWWXXYYZZ112233445566 A two-word MfgInfoC Write MAC sequence, which is programmable using ManufacturerAccess() 0x0035 Security Keys, is required to enable writing these registers during SEALED mode. Refer to the description in Manufacturer Info C for further details. |