SLUUCN4A January 2023 – February 2024
In addition, when [RUNTIME_DEGRADE] = 1, runtime counted when Cycle Count is above Cycle Count Start Runtime can be used as a selector for voltage degradation. There are four programmable stages/levels of rungtime based degradation modes:
NORMAL mode (Accumulated Runtime ≤ Runtime Threshold for Mode 1)
Degradation Mode 1 (Accumulated Runtime > Runtime Threshold for Mode 1 and ≤ Mode 2)
Degradation Mode 2 (Accumulated Runtime > Runtime Threshold for Mode 2 and ≤ Mode 3)
When the configuration bits [RUNTIME_DEGRADE], [CYCLE_DEGRADE], and [RTORCC] are all set, then degradation occurs according to the runtime or cycle count criteria first met.