Use the following instructions to perform output the hot-short test:
- Set the jumper setting on EVM to default position as shown in Table 5-1.
- Set the input supply voltage VIN to 12V and current limit of 10 A.
- Enable the power supply.
- Now, short the output, That is, VOUT to GND with a shorter cable and observe the short-circuit response of TPS1211-Q1 using an oscilloscope.
#T5536460-73 shows hot-short response of TPS1211-Q1 on TPS1211Q1EVM Evaluation Board.
Figure 5-9 Output Hot-Short Response of TPS1211-Q1 Device