The BQ28Z620 includes
the following
new
functions
to synchronize filtered RSOC, RemainingCapacity, and FullChargeCapacity to
unfiltered values when an OCV is taken.
- A new data flash bit [SYNC_AT_OCV]
- If
[SYNC_AT_OCV] = 1, the filtered values are
synchronized to the unfiltered values when an OCV is taken.
- If [SYNC_AT_OCV]
= 0, the values are not synchronized when an OCV is
taken.
- A new command AltManufacturerAccess() SmoothSync() to synchronize
filtered RSOC, RemainingCapacity, and FullChargeCapacity to unfiltered values
when an OCV is taken.
TRM changes include Section 8.6, Section 15.3.1, Chapter 16.