SLUUCP8 June 2024 BQ41Z50
Class | Subclass | Name | Type | Min | Max | Default | Unit |
---|---|---|---|---|---|---|---|
Calibration | Interconnect Resistance | Cell 4 | I2 | 0 | 1000 | 0 | mĪ© |
Description: This is the interconnect resistance value entered by the user that represents the interconnect resistance between the top of Cell 3 and the bottom of the Cell 4, plus the interconnect resistance of the connection from the bottom of Cell 4 to the gauge. The measured CellVoltage4() is compensated for the voltage drop introduced by this resistance.