SLUUCP8 June 2024 BQ41Z50
This command enables/disables the LED display function to ease testing during manufacturing. The initial setting is loaded from Mfg Status Init[LED_EN]. If the ManufacturingStatus()[LED_EN] = 0, sending this command will enable the LED display and the ManufacturingStatus()[LED_EN] = 1 and vice versa.
In UNSEALED mode, the ManufacturingStatus()[LED_EN] status is copied to Mfg Status Init[LED_EN] when the command is received by the gauge. The BQ41Z50 device remains on its latest setting prior to a reset.