The upper section of the Programming screen is
used to initialize the device by loading the default .srec into the flash memory (see Figure 1-9).
- Search for the .srec file using the Browse button.
- Press the Program button and wait for the
download to complete.
- The updated version should be displayed on the left dashboard window within 2
minutes after programming has been completed. If not, reboot BQStudio.
- It is recommended to reboot
BQStudio
after programming the new firmware.