Use the following to set up the EVM testing software:
- On the computer connected to the
EV2400 interface board, launch Battery Management Studio (BQStudio). Select
Charger as seen in Figure 4-1.
- Select the appropriate
configuration file based on the device BQ25638x from the window shown in Figure 4-2.
- Choose
,
on the window that appears, and the main window of the BQ25638x EVM software
appears, as shown in Figure 4-3.