SLUUCR2 October 2023 TPSM843620
Figure 3-16 and Figure 3-17 show the start-up and shutdown waveforms using EN. In Figure 3-16, the input voltage is initially applied and the output is inhibited by pulling EN to GND. When the EN voltage is increased above the enable-threshold voltage, the start-up sequence begins and the output voltage ramps up to the externally set value. Figure 3-17 shows EN shutdown with no load.
Figure 3-18 shows EN start-up with a 6-A load.
TP11 for EN can be used to test the EN start-up. EN is high if there is power, and is low if tied to AGND.