SLUUCR7A January 2023 – December 2023
Because both the QFN and SOT583 packages have the same pinout, there is also the possibility for board designers to overlap both package footprints like in Figure 2-1. This overlap gives more flexibility to switch between packages when there is shortage in supply of one. The TPS62830xRZEREVM does not have this overlap and is only designed for the QFN package.