SLUUCT0A may 2023 – june 2023 TPS923652 , TPS923653 , TPS923654 , TPS923655
Figure 5-14, Figure 5-15 show the hybrid dimming waveforms at 10%, and 20% duty cycles, respectively. Input voltage is 24 V, with 15 white LEDs in series used as load. The full-scale LED current is set at 2 A. The ADIM/HD pin is always low. The frequency of the input PWM signal at the PWM/EN pin is 20 kHz.
When the hybrid dimming is enabled, the LED current is regulated by the analog dimming at high brightness level (12.5% ~ 100%) and by the PWM dimming at low brightness level (0%~12.5%).
Figure 5-13 gives the test result of linearity of hybrid dimming, in comparison with the theoretical value. Input voltage is 24 V, with 15 white LEDs in series used as load. The full-scale LED current is set at 2 A. The frequency of the input PWM signal at the PWM/EN pin is 20 kHz.