All trademarks are the property of their respective owners.
The TPS2117EVM is an evaluation module for the TPS2117 low IQ power multiplexer. The TPS2117 is a dual-input, single-output device that can be configured for automatic or manual switchover. The low quiescent current makes the TPS2117 ideal for systems with a battery supply as an input to extend the life of the battery when in use.