The bench setup diagram includes the function generator and oscilloscope connections.
Use the following connection procedure and refer to Figure 4-1.
For the UCC27332Q1EVM, the connection procedure is as follows:
- First, make sure the output of the function generator and power supplies are disabled before connection.
- Apply function generator channel-A positive on IN and negative to GND.
See in Figure 3.1.
- Power supply #1: positive node connected to input of DMM #1 and DMM #1 output connected to test point marked as VCC, negative node of Power Supply #1 connected directly to test point marked as GND; see in Figure 4-1.
- Connect oscilloscope Ch-1 probes to test points marked as Gate and GND, smaller measurement loop is preferred; see in Figure 4-1.