SLUUCU2A March 2023 – September 2023 UCC14130-Q1 , UCC14131-Q1
The UCC14131-Q1 is the default IC used in the UCC14131EVM-070 but any of the alternate versions listed in Table 1-1 can be used for evaluation. Each of the component versions listed in Table 1-1 are pin-to-pin compatible, functionally equivalent, drop in replacements with respect to one another.
General Part Number | Orderable Part Number | Isolation/Surge/Working Voltage |
---|---|---|
UCC14131-Q1 | UCC14131QDWNQ1 | 5 kVRMS/10 kVPK/1 kVRMS |
UCC14130-Q1 | UCC14130QDWNQ1 | 3 kVRMS/6.5 kVPK/850 kVRMS |
If U1 replacement is required, then TI recommends to always use best practice soldering techniques. Techniques can include taking appropriate ESD precautions and having qualified personnel, skilled at surface mount soldering and board level rework, removing and installing U1. Visually verify the desired UCC1413x-Q1 component version is properly installed in the EVM. If rework on U1 has previously been performed, then visually verify correct orientation of U1 according to Figure 1-1. The pin 1 identifying dot on top of the IC package is oriented at the top left according to Figure 1-1.