SLUUCU3 November 2023
The TPSM8S6C24 leaves the factory settings pre-configured. The factory default settings for the parameters can be found in the data sheet. If configuring the EVM to settings other than the factory defaults, then use the software described in Section 2.2.1. Make sure the input voltage is applied to the EVM prior to launching the software so that the TPSM8S6C24 can respond to the GUI and the GUI can recognize the device. The default configuration for the EVM to stop converting is set by the EN resistor divider to a nominal input voltage of 4.22 V. Therefore, if the user wants to avoid any converter activity during configuration, then apply an input voltage less than 4.22 V. TI recommends an input voltage of 3.3 V.