SLUUCU3 November 2023
The following warnings and cautions are noted for the safety of anyone using or working close to the TPSM8S6C24SEVM-1PH. Observe all safety precautions.
![]() | Warning | The TPSM8S6C24SEVM-1PH circuit module can become hot during operation due to dissipation of heat. Avoid contact with the board. Follow all applicable safety procedures applicable to the laboratory. |
![]() | Caution | Do not leave the EVM powered when unattended. |
The circuit module has signal traces, components, and component leads on the bottom of the board, which can result in exposed voltages, hot surfaces, or sharp edges. Do not reach under the board during operation.
The circuit module can be damaged by overtemperature. To avoid damage, monitor the temperature during evaluation and provide cooling, as needed, for the system environment.
Some power supplies can be damaged when applying external voltages. If using more than one power supply, check the equipment requirements and use blocking diodes or other isolation techniques, as needed, to prevent damage to the equipment.
The communication interface is not isolated on the EVM. Be sure no ground potential exists between the computer and the EVM. Be aware that the computer is referenced to the battery potential of the EVM.