SLUUCV0B August 2023 – April 2024 TPSM8287A06 , TPSM8287A10 , TPSM8287A12 , TPSM8287A15
The TPSM8287Axx EVM GUI is provided on the TPSM8287A12BBSEVM tool folder to communicate with the device over the I2C bus through the USB2ANY adapter EVM. A valid input voltage must be applied.
The GUI automatically connects to the EVM. If this does not happen, then click either the Connect button at the top right of the GUI or the link symbol at the very bottom left of the GUI.