SLUUCV2A October 2023 – November 2023
The following waveforms show the resonant current sense resistor voltage: switch node voltage during startup. 115 VAC, 60 Hz is applied initially to the AC input, then the 390 VDC input is applied to the DC input.