SLUUCV6 June 2024 BQ2969
The BQ2969 circuit module contains the BQ2969 IC and related circuitry to demonstrate the features of the IC. The board does not control current, the OUT signal passes directly to the TP2 connector. TP2 has no current limit or ESD protection on the signals, provide any necessary protection during evaluation external to the EVM. J2 provides a method to separate the supply feed from the input terminal block to measure current or to apply a voltage for customer test mode. Other components provide support for the IC and connections to the board. Basic operation is described in Section 2.1. For details of the circuit, refer to Section 3.1.