The chemistry file contains parameters
that the simulations use to model the cell and the operating profile. A critical
issue is to program a Chemistry ID that matches the cell into the device. Some of
these parameters can be viewed in the Data Memory section of the Battery Management
Studio.
- Press the Chemistry button
to select the Chemistry window.
- The table can be sorted by
clicking the desired column. for example: Click the Chemistry ID column
header.
- Select the ChemID that matches
your cell from the table (see Figure 5-4).
- Press the Program Selected
Chemistry button to update the chemistry in the device.
- Press Program from GPCRB
file button to program the Chemdat file exported from the GPCRB
tool (low temperature optimization tool).